Tool/software: WEBENCH® Design Tools
I'd like to know the efficiency value.
Which is correct?
From the Page 5,(simulation) the efficiency value is 76.189%.
From the Page 2(graph), the efficiency value is above 90%.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software: WEBENCH® Design Tools
I'd like to know the efficiency value.
Which is correct?
From the Page 5,(simulation) the efficiency value is 76.189%.
From the Page 2(graph), the efficiency value is above 90%.
Hi Miyanaga,
The WEBENCH design above shared has an Efficiency value of 76.6% in the operating table for a Load current of 1.3A. The same has been shown in the graph.
Please note that you can change the Iout value in the operating values table and click on Recalculate and corresponding efficiency value will be reflected in the table.
Thanks & Regards,
Praveen