• TI Thinks Resolved

TIDA-00170: TIDA-00170:

Prodigy 10 points

Replies: 1

Views: 21

Part Number: TIDA-00170

Hi,

we are developing a IO product using ADS8688 with TIDA-00170 as the reference, for efficiency, appreciated if you provide the sample code also.

Best Regards

George Yao

  • Hello George,

    sorry for the late reply.

    TIDA-00170 is based on TIVA-C platform, which we are not supporting anymore for industrial applications. we recommend moving to Sitara processors instead.

    However, it is possible with little tweaking to use the standard EVM SW (which is highly recommended as it is well maintained) for ADS8688 by connecting the SPI signals behind the isolator. please check the EVM user guide and if you face issues using the EVM SW let us know.

    Best Regards,

    Ahmed