Hello,
I have made hardware as TIDA-010042 design as is.
I have connected 12amp 7ah battery(C35) and 24watt DC led light for the load and for the solar panel I am using 14V 4ah PSU.
Whenever I am staring at the MCU then power supply giving a supply @ 2.5A and then after 6 to 7 minutes load gets disable due to battery cut off voltage.
After that battery takes a current of only 100mA and load still disabled. But in some time Battery voltage increases and that time load try to enable.
Withing moment load is going disable and battery voltage is going lower to 5V.
I have two questions.
1. why battery voltage is going higher and get lower at the moment?
2. Why load get enable and get disable suddenly? I have also checked using breakpoint at Battery reconnect counter but it is not going inside that loop.
Please help me what could be the problem
Regards
Pulkit