Part Number: PMP4334
Hi everyone,
I have two questions for you regarding the circuit in this reference design (PMP4334). The first one is regarding the linear regulator composed by Q1, ZD4 & R17. The circuit is just there to keep the voltage regulation of U1 within specification. I noticed that this circuit was not included in the final assembly of PMP4334, instead R39 (0 ohm resistor), was placed. If I want to include the linear regulator I would just need to exclude R39 right?
My second question is related to the output voltage. The PMP4334 as is, has an output voltage of around 50V. If I'd implement it with an output voltage of around 24V I would just need to play with R46 and R44 right? Those are there setting the value for the 2.5V comparator U2-A. Can you foresee any other implications for the transformer or any other part of the circuit if I tune it down to 24V?
Thank you very much in advance for your answers and time.
Best regards,
José