Part Number: PMP20183
Hello,
I am unfamiliar with PMP20183 topology, but need a high voltage source running at low current, and this design seems to fit my needs. However, I would like to run it 10% lower than 200V (because of the max voltage of my photodiode that this will be driving), so 180V. Do I only need to drop the feedback resistor R2, R100 and R3 down to a total resistance of 887k? Or are their other considerations to take into account?
Thanks,