Part Number: TIDA-01622
hi
where do I find the value of Kdera, which is the GaN voltage derating?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TIDA-01622
hi
where do I find the value of Kdera, which is the GaN voltage derating?
Hi, Ketan
Thanks for your question.
We will reply to you as soon as possible.
Hi,
for derating, basically, this is customize decision based on application and reliability, the one we use here is a 650V GAN, normally at least 90% derating required.
as ACF can reduce voltage stress on both switch, this should create a higher voltage derating margin than conventional flyback..
BR
Max Wang