This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TI PSPICE ERROR(ORPSIM-15108): Subcircuit undefined

Other Parts Discussed in Thread: LM27403

Hi all,

I am having issues getting TI PSpice to simulate a part downloaded from the  TI website. More specifically, the LM27403 transient model that can be found here: 

I have included the .LIB file inside the Simulation Settings Configuration Files and added the .OLB file to the Design Resources Library folder. Also included is my error log. Please let me know what steps I missed and how to fix the problem.

Thank you,

Filipe

PSPICE ERROR LOG.txt
*Libraries: 
* Profile Libraries :
* Local Libraries :
* From [PSPICE NETLIST] section of C:\SPB_Data\cdssetup\OrCAD_PSpiceTIPSpice_Install\17.4.0\PSpice.ini file:
.lib "\Downloads\snvm503b\LM27403_PSPICE_TRANS\LM27403_TRANS.LIB" 
.lib "nom_pspti.lib" 
.lib "nom.lib" 

*Analysis directives: 
.TRAN  0 1000ns 0 
.OPTIONS ADVCONV
.PROBE64 V(alias(*)) I(alias(*)) W(alias(*)) D(alias(*)) NOISE(alias(*)) 
.INC "..\SCHEMATIC1.net" 



**** INCLUDING SCHEMATIC1.net ****
* source PSPICE STUDY BSR
X_U1         N02903 N02890 N01662 N02993 N02989 N01916 M_UN0001 M_UN0002 N00738
+  N00544 0 N00878 N01122 N01052 N01115 N00935 M_UN0003 M_UN0004 M_UN0005
+  M_UN0006 0 N01532 0 N01332 LM27403_TRANS PARAMS:  STEADY_STATE=0
V_Vin         N00290 0 17Vdc
C_Cdd         0 N00878  10u  TC=0,0 
R_Rf         N00544 N00290  2.21 TC=0,0 
X_Cin    0 N00290 SCHEMATIC1_Cin 
X_Cf    0 N00544 SCHEMATIC1_Cf 
R_Rpgood         N00878 N00738  56.2k TC=0,0 
D_Dboot         N00878 N00935 Dbreak 
C_Cboot         N00935 N01052  100n  TC=0,0 
M_M1         N00290 N01115 N01111 N01111 MbreakN           
M_M2         N01111 N01122 0 0 MbreakN           
R_Rotp         0 N01332  86.6k TC=0,0 
C_Cotp         0 N01332  100nF  TC=0,0 
Q_Q1         N01532 N01532 0 QbreakN 
C_C1         0 N01532  1.2n  TC=0,0 
C_Css         0 N01662  47n  TC=0,0 
C_Csby         N02890 N02903  100p  TC=0,0 
R_Rfadj         N01916 0  66.5k TC=0,0 
L_L1         N01111 N02093  10uH  
R_Rs         N01111 N02100  6.34k TC=0,0 
R_Rcs         N02903 N02100  2.94k TC=0,0 
C_Cs         N02100 N02093  220n  TC=0,0 
R_Rset         N02890 N02093  2.94k TC=0,0 
C_Cc1         N02989 N02985  3.3n  TC=0,0 
C_Cc2         N02989 N02993  390p  TC=0,0 
R_Rc1         N02985 N02993  3.16k TC=0,0 
R_Rfbb         0 N02993  4.42k TC=0,0 
R_Rfbt         N02993 N02093  20k TC=0,0 
R_Rc2         N02993 N03134  53.6 TC=0,0 
C_Cc3         N03134 N02093  470p  TC=0,0 
C_Cout         0 N02093  10u  TC=0,0 
** Floating/unmodeled pin fixups **
R__UC0001   M_UN0001  0   {1/GMIN}
R__UC0002   M_UN0002  0   {1/GMIN}
R__UC0003   M_UN0003  0   {1/GMIN}
R__UC0004   M_UN0004  0   {1/GMIN}
R__UC0005   M_UN0005  0   {1/GMIN}
R__UC0006   M_UN0006  0   {1/GMIN}

.subckt SCHEMATIC1_Cin 1 2  
C_Cin         1 _SR C_Cin 10u  
.model         C_Cin CAP C=1      
RESR_Cin         _SR 2 5m   
.ends SCHEMATIC1_Cin

.subckt SCHEMATIC1_Cf 1 2  
C_Cf         1 _SR C_Cf 1u  
.model         C_Cf CAP C=1      
RESR_Cf         _SR 2 1m   
.ends SCHEMATIC1_Cf

**** RESUMING Test.cir ****
.END


ERROR(ORPSIM-15108): Subcircuit LM27403_TRANS used by X_U1 is undefined