Hello,
I like to use TIDA-00640 Reference Design to monitor, Voltage & Current, of individual solar panels that are connected in series and in parallel.
I appreciate your response on the following questions:
1. Is this reference design appropriate for the above application?
2. Can I add a MOSFET on the "hot " or "return" line?
3. Is there a tool that I can use to simulate the design?
I look forward to hear back from you on the above three questions.
Regards,
Raymond Koosha