Other Parts Discussed in Thread: TIDM-1000
Dear all,
I am trying to debug the TIDA-01606 boards: Power CardE2; Gate DriverE2 cards; F2837D controlCARD R1.3.
I think I have managed to understand how to use the test points on the power card and gate drivers and to identify the function of all LEDs, however I saw there are test points on the control card R1.3 as well but I couldn't find out how to use them, it seems most of them are not even connected to the control card's circuit.
I was wandering if there is any specific documentation regarding TIDA-01606 PCBs debugging. I checked all datasheet, however they do not contain complete information on how to debug the system.
To be more specific, I would like to know:
- How can I debug the gate driver boards?
- Check power supply levels
- Check PWM control signals
- Check fault upon desaturation signal (FLT)
- Check ready signal (RDY)
- Check reset signal (RST); how can I send reset signal?
- How can I debug the Power CardE2?
- Check power supply levels
- Any other test that can be done to assess correct operation of the board
- How can I debug the Control Card R1.3?
- What is the function of the test points?
- TP1; TP2; TP3; TP4; TP5; TP6; TP7; A:TP1; A:TP2.
- How to use the test points
- What is the function of the test points?
Please let me know. Thank you in advance.
Sincerely,
Adriano Arci