Other Parts Discussed in Thread: MSP430FR2355
Hello,
I am working an TIDA-010056 Evaluation board for running a BLDC motor.
For data monitoring, I wish to use UART module and capture data via RS-232.
Working previously on TIDA board due to some issue (not found yet) my LDO stopped working so I am supplying 3.3V and GND externally via either PC or DC power supply.
My issue regarding UART pins is, I am not available to receive data via UART. I have captured data image from UART via oscilloscope and shared below.
Also to find if my code is proper, I have dumped same code in an MSP430FR2355 Launchpad and i could see the data via UART is proper without any issue.
Please find the same image below.
EVM_UART image:
Launchpad_UART image: