• Resolved

TIDA-00961: PCB supplier in Japan

Expert 3245 points

Replies: 6

Views: 60

Part Number: TIDA-00961

Hi sir,

I an interesting in reference design TIDA 00961.

I want to make the board with the exposed Gerber data of the reference design TIDA 00961,

and I was told that it cannot manufacture because of the overseas standard from two Japanese PCB board manufacturers.

Could you introduce a PCB manufacturer supplier?

Thanks.

  • Hi, Frank

    Not understand your problem about 'the overseas standard'. And, I do not see any special design  in the PCB of TIDA-00961. 

    Dyson Guo

  • In reply to Desheng, Guo:

    Hi Dyson,

    Thank you for your response.

    the problem is gerberdata unit, the gerberdata unit of TIDA-00961 in public is mil, 

    but customer need mm unit for the gerberdata.

    Can you transfer it from PCB design file?

    or can you provide PCB layout design files?

    you can also send it to my email if this is not in public.

    X1054259@ti.com

    Thanks.

     

  • In reply to FRANK1:

    Thank you in advance, waiting your feedback.

  • In reply to FRANK1:

    Hi, Frank

    This is minor issue, most PCB vendor could translate the unit by themselves.

    If not, you could generate geber file with the PCB file (altium designer format), or send the PCB file to vendor directly.

    Dyson Guo

  • In reply to Desheng, Guo:

    Thank you

  • In reply to FRANK1:

    Hi, Frank

    please refer below URL:

    Dyson Guo