Part Number: PMP7763
Hi Team,
The PMP7763 reference design shows that it can operate from 30V-800VDC input supply. The datasheet of the T100 transformer shows that it's turns ratio is 8:1 which translates into 30V/8 = 3.75V output from a 30V input. A customer wants to know how it is possible to output 24V from a 30V input if the transformer turns ratio is 8:1?
Regards,
Danilo