Other Parts Discussed in Thread: C2000WARE, AMC1306M05, TMDSCNCD28379D
Hi Team, we need your inputs about this implementation.
1. Tried to multiply 2 variables of 16 bits (defined Uint16 in the code) and receiving the result to a 32 bit variable (defined Uint32 in the code). The result I received in the 32 bit variable was only the 16 LSB bits of the multiplication result.
How can I get the full 32 bits result to my 32 bit variable? Should I define the 2 16bits variables also as 32 bits?
2. In TIDA-01606 design I receive from amplifier AMC1306 a PWM signal in a constant frequency with changing duty cycle. I need to find the current duty cycle using F28379D LaunchPad. I wanted to use Capture port in order to do it (eCAP port), but I didn't find any information regarding it.
Can you give me an example of using Capture port to find PWM duty cycle?
A code example will be very helpful but any other information will help as well.
3. Read about sigma delta modulator, and I didn't understand it quite well.
As I understand it in TIDA-01606 I need to read the information from some amplifiers using sigma delta modulator.
Can you elaborate about it in more details? Can you explain me what is the use of it and which amplifiers should work with it?
Can you give me a code example of using it?
4. Do you have code files to implement for TIDA-01606
Thank you very much in advance.
Regards,
Mark