I have an instantaneous power loss signal.
I would like to calculate the average power of its.
This guide say, that the average power can be performed using integration S function in PSpice.
Single-Switch-Forward-Converter-App-Note_Final.pdf (pspice.com)
Chapter Switching Losses in MOSFETs
It seems, it should work as in the picture here:
Here are my results:
You can see, that the value has to be about 100mW as it can be calculated via AVG functions.
Maybe I have mistake understanding this function.
Help definition: "S(x) is integral of x over the range of the X axis variable"
Why does S() not give correct value?
Attila