Other Parts Discussed in Thread: BQ25890, TUSB321, TPS65982, , TUSB320, BQ25703A, PMP40294
What power source was used to test this circuit out when charging the power bank?
I have an Anker PowerPort+ 5 USB-C feeding my BQ25890 charger with TUSB321 requesting 3A and the USB through a DSEL controlled switch.
I get the 3A but no voltage greater than 5V.
I suspect that the D+/D- link in the Anker is fouling the D+/D- handshake for the voltage.
Does this mean I have to use a TPS65982 instead of the TUSB321, or is there a power source that will work?
I note that the USB switch is controlled by the microcontroller in PMP4496 and not DSEL...?