Other Parts Discussed in Thread: ADS1248, ADS1148
Hello everyone,
I am trying to implement the (4 or more) RTD Temperature Measurement circuit where I want it to be at least near about ±0.6°C accurate.
I have a two-parter question related to the TIDA-00110 reference design based on ADS1248:
- Why the two current sources are placed at different points of the RTD i.e. one is placed at the power line (to the RTD) at the positive side and one is placed on the sense line on the negative side, shouldn't they be placed at the same point for better accuracy considering we are using 4-wire RTD?
- The accuracy mentioned in the document is ±2°C whereas the accuracy graph showed later in the same document shows the accuracy is ±0.6°C max if it is ±2°C is there a way to improve it?
Thanks for the help,
Reagards,
Yash RK