Other Parts Discussed in Thread: DRV10983EVM,
Hi,I'm studying the DRV10983EVM,but we need to drive the motor with constant speed even if the motor torque is changed.
I found that TIDA-01496 can drive the motor with constant speed by entering the speed control signal to ADC input of MSP430.
But I'm not sure the relationship between ADC input value and rotation speed(Hz).
according to 3.1.2.2 Flow for Using ADC10 of MSP430 to Implement PI Speed Control System in the manual as below,I think we should define SPEED_INPUT,and scale value.
3. The speed level determines the target speed of the electrical cycle (Hz), defined by SPEED_INPUT,and scale value, defined by Scale.
if we would like to drive the motor with the constant speed of every 1000rpm between 10000rpm~30000rpm ,could you tell me how we could define the value ?
Thanks .