Please note that E2E has undergone a major upgrade. Before logging in, please clear ALL your browser's cache and cookies.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TIDA-00120: TIDA-00120

Part Number: TIDA-00120
Other Parts Discussed in Thread: TIDA-010042

Hi, I am developing a li-ion battery pack with 13S4p 21700 cells, 20Ah 48V and using TIDA010030 for BMS. I also need a matching built-in MPPT charger and I wonder whether the TIDA00120 can be adapted to match the cells as a proof of concept for the first sample builds.

  • Hi Jo,

    thanks for reaching out on TIDA-00120 and welcome to e2e!

    This is a similar question to the thread below,

    As well, Let me direct this question for the appropriate engineer to respond. Let me know if you have any other questions.

    Thanks,

  • Hi Jo,

    TIDA-00120 was designed for 12/24V batteries. You can adapt this design for 48V battery by changing the MOSFETs (and passives) used. However, a quad driver as used in this design may not give good performance. The driver has to be as close to the FETs as possible. You can also take a look at TIDA-010042 to get an idea about the changes that may be required.

    Regards,

    Salil