Hello
I have a major question in refrence to the above refrence design.
When loading one rail of the SMPS output as below, what is the resulting voltages?
Example 1:
Loading the +42V rail with 6A (+ & 0) not loading the -42V rail, what is the voltage at the both rails?
Loading the -42V rail with 6A (- & 0) not loading the +42V rail, what is the voltage at the both rails?
They will remain +-42VDC in such load conditions?
Any answer is really appreciated.