I just created a buck-regulator design using the TPS40192, using one each of CSD16410Q5A, which has Ron=10mOhm@4.5V, for high and low-sides.
I_rms(Q1) was calculated to be 4.05A. The Q1 (high-side) Power Dissipation is 637mW according to SwitcherPro. I don't see how this can be the case because for a MOSFET in saturation, P=I^2.R = 4.05^2*0.010 = 164mW ?? Qg=3.9nC, so that's not contributing much to power dissipation either.
The calculated junction temperature seems to be based upon the 637mW number, so that too seems inflated.
-Wing