Tool/software: WEBENCH® Design Tools
A product of our company uses the SN65HVD75 design circuit, but the TVS is damaged during the customer's use. The design circuit is as shown below (the signal line is not connected in series with 100Ω). Now we are ready to choose between CPDQC12VE-HF and SESD0402X1BN-0015-096. Which TVS do you think is better?