Part Number: TIDA-010039
Hey Team,
Is the TIDA-010039 bidirectional? I see that in the main description of the reference design, that it states bidirectional functionality, but then goes on to say " For design information on the DC/AC implimentation, see TIDA-01606." What should I be looking for to achieve this type of functionality?
If the TIDA-010039 is bi-directional, does it need to be grid-tied when acting as an inverter? Is there a way to tell if one of our designs needs to be grid-tied for operation? I am wondering the same thing for the TIDA-01604.
Thanks,
Dajon McGill