This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

WEBENCH® Tools/SYSCONFIG: Complete Support for TMS320F28075

Part Number: SYSCONFIG
Other Parts Discussed in Thread: TMS320F28075

Tool/software: WEBENCH® Design Tools

Hi,

I am trying to use the pinmux functionality in the SysConfig webtool to choose which pins should be used for which functionality.  I would like to use this as the medium to discuss the configuration with our EE team.

The TMS320F28075 part doesn't seem to be complete on the utility.  I.e. ADCs, JTAG, appear to be missing.  At least when you compare the options against the 280049 option.

Is there anyway that the tool can be updated to define the full assortment of pins?

Thanks,

-Colin

  • JTAG pins should be in the OTHER signal.

    ADC pins other than ADCSOC digital signal is not included in the sysconfig pinmux.

    The normal analog ADC pins are not like other digital signal. Having two ADC inputs used on the same pin does not cause a conflict, thats why they are in the sysconfig pinmux tool.

    BUT we do plan on adding ADC and other analog peripheral functionalities to the tool in the future releases.

    Nima 

  • Hi Nima,

    Thanks for the quick response.  I know that some pins have dedicated peripheral functionality, but having the ability to assign (and label) them lets people use the tool to discuss how all the connections to the part should occur.  This tool is great for the peripheral pins that can move, but you end up with only an incomplete picture of the design as a whole. 

    Consider it a feature request! Thank you!

    -Colin