This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TIDA-020032: Need example code for both BLE and CAN working together

Part Number: TIDA-020032

Hello, 

We are able to run the BLE  for project zero and able to detect it on Android smartphone.

We are able to use a CAN project and send the CAN messages to a CAN simulator PCAN device. 

However, we are unable to find a project code, which does the BLE pairing and also sends the information via CAN. 

Can you point us the example code / document on the same?

Also we would like to receive both RSSI and AoA via CAN when we detect a BLE device on the board. How do we populate these via CAN?