To who it may concern,
I am designing a PCB that will have a signal generator that will send a signal, along several balancing lines, to the main PCB in order for the main PCB to be able to detect a disruption on any of the balancing lines, should the signal not reach the main PCB.
My request is whether you are able to suggest to me any component that acts as a signal generator, along with an MCU to which the component will be connected and I also require an ambient pressure sensor which will be in the main PCB monitoring the pressure inside the battery module.
Summarising everything here is what I need.
1) Signal generator
2) Ambient pressure sensor
2) MCU microcontroller (to be able to control the signal generator, ambient pressure sensor, temperature sensor, and battery monitoring)
They all have to be AEC-Q100 qualified.
Thanks,
Regards,
Giorgio