Other Parts Discussed in Thread: AMC1306M05
Dear All,
When using the current control loop with TINV_LAB 3 there is high oscillation in the output current. We transfered the feedback current to the LEM sensors from the following section,
101 #define TINV_SDFM 1
102 #define TINV_ADC 2
103 #define TINV_CURRENT_LOOP_SENSE_OPTION TINV_SDFM // We used TINV_ADC
- The controlled current became stable and the conclusion from this phenomena is the AMC1306M05 isn't working.
- We checked the clock input and SD_out and found signal (20MHz clock , bit stream) OK.
If the pin Ain and GND_2 should be connected please advice as we found some threads talking about this issue.
Thank You.