It is quite easy to create a new model or part by importing the 3rd party model in a PSpice For TI project but it becomes difficult handling multiple generated models especially when we need to work across different devices as we need to re-generate those same models while simulating the same project file on a different device.
Thus, can anyone please guide me towards a way in which we can create a dedicated library of the generated/created models in PSpice For TI which can be transferred across multiple devices as well as could be easily shared with multiple members of the team working on the same project without having to re-create/re-generate the models in a new device.
Thank You,
Srinjay Bhattacharya