Hi,
In TIDA-010042 board test, I am currently using E-load as a battery pack. While I am charging, there is no voltage at the load output (J7). Then, I checked Q5 and U12. U12 does not get L-EN signal from MCU. So, I checked software. I don't see any issue. The Battery output voltage is higher than Battery reconnect voltage. And Charged current is only 1A. So, still lower than overcharged current limit.
So, is it because of software/hardware or because of E-load? Any suggestion, please.
Best regards,
Yin Min