Other Parts Discussed in Thread: TMP117, LAUNCHXL-CC2640R2,
I have a LAUNCHXL-CC2640R2 and SparkFun TMP117 Temperature-Sensor "Foto 0".
I have connected them together and by using the "Portable Project" from (Simplelink_cc2640r2_sdk-Examples) i was able to read the Temperature values via I2C in the PuTTY Console.
My next Goal is to read the Temperature values via Bluetooth in the app on my smartphone.
Therefor i have imported the TIDA-01624 Software in CCS and then i have tried to build it(sdk 2.20.0.49)
Unfortinlly the build was not completed because of the Errors showin in the screenshoot "Foto 1".
Then i have changed the SDK version to (5.10.0.02) and i have reimported the Project and i have built it again.
The build was also not completed because of the Errors showin in the screenshoots "Foto 2&3".
To temporery get over this Problem i have commented the 2 Lines (109 & 110) which made the Errors and then i built it again. This time the build was sucssfully completed. Then i have connected the LAUNCHXL-CC2640R2 to my PC and i have run the Project.
After that i was not able to find this Project in SimpleLink-SDK-Explorer-App on my Phone and in the PuTTY Console there is nothing to see "Foto 4".
Do you have any Ideas to solve this Problem ?
Is that true that the TIDA-01624 Software was not written to run on the LAUNCHXL-CC2640R2 ?
If that is true, can you tell me if there are any software or Examples that i could use to achive my Goal ?
Thanks in advance
Tareq