Hello,
I am inquiring in regards to a software kit related to the reference design TIDA-00915: Three Phase, Three-phase, 1.25-kW, 200-VAC small form factor GaN inverter reference design for integrated drives. I noticed that there are Development Kits associated with some reference designs in the Resource Explorer inside of CCS. The reference design I am interested in did not appear to have a 'Development Kit' with it for it's associated MCU/DSP: the Piccolo F280049C. I can assume that not all reference designs have an associated Development Kit or I am not able to locate it. Is this the correct assumption or am I just not able to locate it. If there is not a Development Kit associated with it, I noticed there is a Development Kit for the reference design TIDM-HV-1PH-DCAC-Single Phase Inverter-Voltage Source. Would this Development Kit be a good start to being developing software for the TIDA-00915 reference design or do you have another recommendation in the Resource Explorer.
I have a attached a picture of the Resource Explorer as well as the reference design I was referring to. Thank you for your time.
Best Wishes,
Anthony Bristow