Other Parts Discussed in Thread: DLPC150
I have been reviewing the files posted with TIDA-00554 DLP NIR Reference design and have a few questions regarding revisions. The files were all downloaded from:
www.ti.com/.../TIDA-00554
We purchased two complete systems from the recommended supplier (not sure of the purchase details as they were purchased before I started with the company). I have noticed some variations in the numbers on the various boards used in the system. For example, the TIVA board is listed as TIDLP-23328-03 in the silk screen on the physical board, but in the Gerber files provided on the TI website it is listed as "23328-04 NIRscanNano_TIVA_board_gerber". Is the "-04" after the "23328" a revision?
The revisions became more of an issue on the DLPC board:
Within the tidrfm3.zip file, the "2514152_NIRscanNano_DLPC150_ALL_LAYERS.pdf" file on Layer 1 - Primary side appears to match well with the actual board. Similarly the "23327-05_NIRscanNANO_DLPC150_board_gerber" file from the tidcaj7a.zip file appears to match, but when we imported the board layout CAD files from the "23327-04_NIRscanNANO_DLPC150_board" folder in tidrfm4a.zip, the resulting visible layer did NOT match the board and Gerber, with much less of a "pour" around the various points (and therefore much more distance between most traces). Was there a reason for this change? Which one is the newer version (the gerbers in tidcaj7a.zip or the CAD files in tidrfm4a.zip)?
Thanks and regards,
Michael Pliska