Hello support team.
I am trying to run TIDA-00951 software but I am getting errors with CCS and I am not able to start the proyect.
I have used several versions CCS6.2.0, CCS7.0.0 and CCS10.4 and differents pc WIN7 and WIN10, but I can´t get it. I am using XDS110 Debug Probe.
Here you can see an error sample:
**** Build Finished ****
Buildfile generation error occurred..
This project was created using a version of compiler that is not currently installed - 6.4.2 [C2000]:
- See 'Help > Install New Software' and select 'Code Generation Tools Updates' to check if this compiler is available through a CCS update.
- Visit CCS App Center to get the latest compiler support.
- Or download and install the compiler [http://software-dl.ti.com/codegen/non-esd/downloads], then register it with CCS through 'Preferences > CCS > Build > Compilers'.
Build stopped..
And the question is:
What Do I doing bad?
What is it the suitable compiler?
How I can load TIDA-00951 firmware?
Thank you very much for your support.
Awaiting your comments.
Carlos González