I have a question about AWR1843.
I will ask about how the settings made by SW in each system of AWR1843 can be set specifically.
(1) Analog-Sub-System
(1.1) Enable transmitter and receiver
Where can I set the activation? (Not in the AWR1843 documentation)
(1.2) Data mode setting during AD conversion (Real or Complex)
Where can I set it?
(1.3) Setting the number of resolution bits
How do I set 12 bit, 14 bit or 16 bit?
(1.4) Composition of chirp waves
Where can I set it?
Is it possible to set the chirp duration, start frequency, bandwidth, and idle time?
How many seconds can Idle Time be set?
(1.5) Chirp frame configuration
Where can I set the chirp frame?
I want to configure both the chirp frame time and the number of chirps.
How many seconds should the Idle Time between chirp frames be?
(2) Radio Processor Sub-System
(2.1) DFE data storage format
In what order do you store four AWR1843 receivers Rx?
(2.2) ADC Buffer data storage format
-Is the data storage format performed in the order of the chirp frames of each receiver?
-The input data to the ADC Buffer is set from the DFE or HIL from the register. Where can the register be set?
・ Where can I set Single-Chirp mode and Mutii-Chirp mode?
(3) Master-Sub-System
· How do you start or configure the bootloader?
(4) DSP
-I was able to consider using a library to set the FFT process, but should I create the program and write it to UniFlash?
-Where can I set the data transfer between each memory?
Sorry for the very long question.