Other Parts Discussed in Thread: AMC1301
Hi,
We are evaluating TIDA-01606(10-kW, bidirectional three-phase three-level (T-type) inverter and PFC) and TIDA-01000(Vienna Rectifier-Based, Three-Phase Power Factor Correction) reference designs for PFC application.
I noticed, while both the designs use CC2000 series controller, the 3-Level T-Type reference design does not use isolation between the high voltage and the CC2000 controller. On the other hand the Vienna Rectifier-Based uses AMC1301 for sensing the line voltages and the two half DCbus Voltages.
My questions:
1.) Why does the Vienna Rectifier Design need the AMC1301s? Is it possible to get away without the AMCs?
2.) I also saw the Line Voltages being sense this way(non-isolated) in another design, where the C2000 & all the other digital circuitry was powered from a mains isolated powered supply and yet the Line Voltages were connected directly to CC2000 with a simple resister divider, i.e. without any isolation device. This was an energy meter design. I understand that the isolation requirements are specific to an application and the required standards. But It feels like I am missing some fundamental understanding here. Are the CC2000 ADCs (Presumably the differential inputs / Sigma-Delta Modulators) have any built in isolation? If so what is the isolation voltage?
It would be helpful if you can shine some light on what's going on with isolated / non-isolated ways of sensing the high voltages the two cases?
Thanks in advance,
Best Regards