Other Parts Discussed in Thread: LM5163,
Hi there,
I have two questions I hope you can help me with.
1. I noticed for this design the LM5163 Buck is powered off of Cell16+ and not after the fuse. This implies that if there were a short circuit/overload fault with the Buck the fuse would not open and current would continue to flow via the Cell16+ balance connector. Is there any reason for this or was this unintended?
2. I see some redundancy with D47 and the reverse charge circuit of Q29+surrounding components. Is the reverse charge circuit necessary if we have D47? It looks like it would only come into play if D47 were to fail?
Thanks in advance,
Steve