Other Parts Discussed in Thread: TPS61089, TPS61088
We are working to use the TIDA-050039 single solar cell energy harvesting design with microbial fuel cells which have a similar Maximum Power Point profile to single solar cells. We want to adjust the Li-Ion design for 4.5-5.5V (4 x 1.2V cells) NiMH battery charging up to 2 watts (400-500 mA) from fuel cell input at 0.45 volts. We would appreciate suggestions for adjusting TIDA-050039 components, particularly compensation, and advice on expected power conversion limits.