Dear all,
I'm trying to use TIDA-01606 for the grid-connected inverter but it has too high rated power than I can test.
My test power is less than 1 kW, and the input/output voltages are also changed to 200Vdc/100Vac.
Since I need the inverter with high efficiency, I'm planning to change some components.
As far as I know, the twelve switches need to be replaced with low power ones.
Is there any problem if I change them?
Or, is there anything else that needs to be changed?
Thanks in advance.