PSPICE-FOR-TI: SN74AHC1G04 model problem

Part Number: PSPICE-FOR-TI
Other Parts Discussed in Thread: SN74AHC1G04

I am trying to use the SN74AHC1G04, but when I run the model I get the following errors. I believe its caused by line 115

.PARAM MAXICC = maxICC

I see some other models have also suffered the same issue, please fix it

========================= Simulator output ============================================

--------------- INFO(ORPROBE-3209): Simulation Profile: SCHEMATIC1-bias ---------------
INFO(ORPROBE-3183): Simulation running...
** Profile: "SCHEMATIC1-bias" [ C:\Users\gary\Documents\Pspice Ti\gan_ring_osc-pspicefiles\schematic1\bias.sim ]
Reading and checking circuit
WARNING(ORPSIM-15223): Library file C:\Users\gary\AppData\Roaming\SPB_Data\cdssetup\pspTILibDir\SN74AHC1G04.lib has changed since index file nom_pspti.ind was created.
WARNING(ORPSIM-15227): The timestamp changed from Wed Oct 13 14:17:14 2021 to Sat Apr 4 05:01:50 2020.
INFO(ORPSIM-15422): Making new index file nom_pspti.ind for library file nom_pspti.lib.
Making index file for library C:\Users\gary\AppData\Roaming\SPB_Data\cdssetup\pspTILibDir\nom_pspti.lib
Please be patient. This may take several minutes...
ERROR(ORPSIM-16152): Invalid number: Error while converting token 'maxICC' to double value. Token can be a constant or expression
ERROR(ORPSIM-16152): Invalid number: Error while converting token 'maxICC' to double value. Token can be a constant or expression
ERROR(ORPSIM-16152): Invalid number: Error while converting token 'maxICC' to double value. Token can be a constant or expression
ERROR(ORPSIM-16152): Invalid number: Error while converting token 'maxICC' to double value. Token can be a constant or expression
Circuit has errors ... run aborted
See output file for details
INFO(ORPROBE-3188): Simulation aborted