Part Number: TIDA-00817
I am working on a BMS design using BQ76PL455A-Q1 battery monitor and BQ34Z100 fuel gauge. The existing reference design of the single 16 cell monitor was extended in my use case for a 32s8p configuration. The design shows an excess current draw when the base battery monitor wakes-up receiving the pulse. I tried using a higher value resistance of 100ohm instead of 49.9ohm for the wakeup pin to debug the issue. Can you tell me if there are any changes to be done to the design tida-00817 when extended to stacked up designs, given that the entire circuitry works fine when only the battery monitors (not along with fuel gauge) are operated through a wakeup pulse.