Hi,
We have a BMS which is nearly the same as TIDA-00792 EVA Board. We generally use this BMS in the 7S and 14S lithium battery configurations. In this case, the protections and all other functions work as they should.
In our application, the BMS outputs are connected to an inverter (AC to DC converter). Naturally, at the first connection, the inverter draws a high inrush current and the BMS enters the short circuit protection(SCP in discharge). The problem starts at this point.If the battery pack is in 14S LFP configuration, the SCP protection is activated just in time and protects itself. However, if the battery is in 15S LFP configuration, the discharge mosfets burn before the protection activates. In the measurements we made after the failure occurred, we detected that the gate-source-drain pins of the discharge mosfets were short-circuited to each other.
Do you have any comments on what changes with connecting the 15th battery?
Thanks in advance
Best regards.