This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DC/DC bidirectional isolated low power converters



Hello,

I'm looking for a few convertersin the following 2 specifications:

Here're the couple of types of converters i'm looking for: 1) I'm looking for low power isolated bi-directional converters for testing out active cell balancing on some new cell designs developed at NREL and other DOE labs.

The specs are: a) Vin 2 - 5 V: , Vout: 2-5 V (higher is fine as long as minimum Vout is less than 5); Power = (1- 10 W) Current: 1 mA - 2 A range)

2) Another isolated bi-directional dc-dc converter up to 40-50 V output. current range (1-10 A). Vin: 5-10 V.

thanks,

Ram