What does the circled field actually sets? Is it the deviation parameter? If yes what happens to the gaussian curve as I increase the parameter from 1 to 9 ?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
What does the circled field actually sets? Is it the deviation parameter? If yes what happens to the gaussian curve as I increase the parameter from 1 to 9 ?
Hi Ajay,
According to the PSpice User Guide, this is a Gaussian distribution GaussUser which has a default sigma value of 1.When this is selected, user can see the value of sigma displayed alongside. The sigma value can be changed from 1 to 9.
More information about Monte Carlo simulation can be found in the user guide. Please click Help -> PSpice for TI Help to view the User Guide. You can find and view additional information, such as the reference guide, under Help -> Documentation.
Thank you,
Jackie