Dear TI team,
Good morning.
We have sensing DC panel voltage in which we have used DC voltage sensing reference circuit from TIDA-01606.
Kindly find below details.
For example we are sensing DC panel voltage of 400V at no load in converter and We have ADC value 850mV.
After above step we have step up the voltage to 600V and loaded the converter with 1A.
Then even though input voltage is 400V constant,we are getting ADC value of 1V .(850mV+150mV)150mV is getting added.
Kindly reply.
Thank you,
Girish K
Caliber