Hi Experts,
Good day.
Client is producing an inverter for compression for air condition and need to rebuild it.
It is THGA 5512C 400 – 440V/50 – 60Hz.
Rated current RLA 1,7/1,8A
Max. current 2,5/2,5A
Start current LRA: 10,7/11A
Compressor is feeded from bus net 28V. To prevent of current shocks during the start, they plan to make a linear incidence start for 2 seconds. Their customer needs a new inverter for electrobusses for feeding air condition with power output 17KW.
Question: Is it possible to make this development on our kit (TIDA01606), is it suitable?
Thanks for your guidance.
Regards,
Archie A.