This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TIDM-1007: Totem pole Bridgeless PFC Design in Webench

Part Number: TIDM-1007

Hello,

We are referring TIDM-1007 for AC-DC PFC design. We wanted to do some modifications in the design using your power design tool i.e. Webench

In AC-DC designer using these parameters:

  1. Vin_Min = 90 VAC
  2. Vin_Max = 270VAC
  3. Vout = 400VDC
  4. Iout = 9A
  5. Ambient Temp = 30C

After adding above details in the webench I am getting the results of simple PFC Boost Converter but I want the design with Totem Pole Bridgeless PFC topology.

Looking forward for your expert support.

Thanks and Regards,

Vikas Dwivedi

  • Hi Vikas,

    I'm not quite sure about your question. Do you want to know if TIDM-1007 is good for your specification?

    Best,

    John

  • Hello John,

    Thank you for your reply.

    I just wanted to create the Totem Pole Bridgeless PFC topology in webench for above specifications. When tried to do that I got the results for simple PFC boost converter in webench and not the Totem Pole Bridgeless PFC.

    So my question is how to generate the design of Totem Pole Bridgeless PFC topology in webench? It will help me to redesign the TIDM1007 for our requirement.

    Thanks and Best Regards,

    Vikas Dwivedi

  • Hi,

    If this question is specifically related to Webench,  we need Webench expert to answer this.

    Let me pull them for the support.

    Best,

    John

  • Hi Vikas,

    Thanks for trying out Webench and reaching out to us. Kindly note that, currently webench do not support Totem Pole Bridgeless PFC design. As you have observed, Webench only supports simple PFC boost right now. Only alternative I see here is using TIDM-1007 reference which you have mentioned.

    Kind Regards

    Bhushan