This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TIDM-1007: Totem pole Bridgeless PFC Design in Webench

Part Number: TIDM-1007

Hello,

We are referring TIDM-1007 for AC-DC PFC design. We wanted to do some modifications in the design using your power design tool i.e. Webench

In AC-DC designer using these parameters:

  1. Vin_Min = 90 VAC
  2. Vin_Max = 270VAC
  3. Vout = 400VDC
  4. Iout = 9A
  5. Ambient Temp = 30C

After adding above details in the webench I am getting the results of simple PFC Boost Converter but I want the design with Totem Pole Bridgeless PFC topology.

Looking forward for your expert support.

Thanks and Regards,

Vikas Dwivedi