Other Parts Discussed in Thread: PMP, PMP11228
Hello,
I want to design a capacitor charger.
The input is 18-36V, Output voltage is 42V, output current is 0.9A and output capacitance is 27mF.
Also output current and voltage must be measured due to output capacitance estimation.
Input voltage is relay controlled, so it rises very fast, PMP8711 boost converter with diode may cause high inrush.
Can you help me which topology and TI IC best fits with this application?
Regards,