Other Parts Discussed in Thread: UCC27511, UCC27512, UCC27710, TLV760
Hello Sir,
I have several Queries.
1. Can I use IC no. UCC27512MDRSTEP instead of UCC27511DBVR? If so, what will be the output resistor's value instead of R26 (3.3 Ohm) and R27 (1 Ohm)? [Note: As instead of Split output OUTH and OUTL , UCC27512MDRSTEP has only one output. What will be the value of that output pin resistor?)
2. Can I replace TL431AIDBZR with TL431LIAQDBZRQ1 keeping other parameter same?
3. What will be exact replacement of IC TPS7A1601DGNT (LDO) and UCC27714D(High side, Low side Gate Driver) which are available in TI now? If need to change some external components for this replacement what those will be?
Please guide me with the above queries.
Thanks