This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TIDA-00951: SW and transformers

Part Number: TIDA-00951

Dear all.

This forum has many topics about software and specifications for transformers, but I did not find information in public.

Can you help me by sending information about T1 (750343383R00), T2 (750343382R00) and T4 (750343341) transformers?

Also I need the TIDA-01281 board FW for TIDA-00951 application. Can you send me binary file, or source codes better?

  • Hi Dmitriy

    TIDA-00951 is an old solution and the designer has left the team.

    Considering the requirements from customers, I think the most suitable solution is TIDM-02002 which has advantages of 1: This topology can be operated with soft-switching on both side; 2: this topology is much popular and well understanding than TIDA-00951. So I recommend you to reference TIDM-02002 for better performance and support. And I suggest you to open a new E2E post if any questions regarding TIDM-02002 and that will lead them to the right owner for support.

    At last, thanks you for your understanding and support.