Hi,
is it possible to have a pwl signal controlled current that is triggered to start by a voltage signal from another part of my simulation?
i have a certain part of my simulation that goes from 0 to 1.8V at a certain point in time, and a current generator with a piecewise linear signal for my desired waveform, but can't figure out how to connect them such to make the waveform start only after the 1.8V
i thought perhaps the VCCS (seperate controlling component) maybe could be used, but not sure.
Thanks,
Michael.